Home

Over the past decade building automation has continued to play a greater role in reducing energy costs and carbon emissions in facilities around the world. Much of this increase in efficiency can be attributed to today's advancements in system monitoring and control technologies. At the heart of these advanced and innovative systems are ADIs signal processing ICs that include A/D and D/A converters, amplifiers , power management, RFICs and so much more. ADI has the system level expertise and products to help make your building system design the best it can be.

Content on this page requires a newer version of Adobe Flash Player.

Get Adobe Flash player

  • Building Control and Automation
  • Today's sophisticated buildings require a higher level of energy efficiency, safety and comfort than ever seen before. To obtain peak operating performance in all of these areas simultaneously requires a complex and reliable network of accurate sensors and monitoring /control systems . Analog Devices offers an array of high performance reliable, signal processing solutions that make all of this possible. More...

  • LED General Lighting
  • LED's are becoming the preferred lighting technology in the industrial, office, and residential segments not only due to their high efficiency but also because they enable smarter lighting systems. Analog Devices is driving advanced features and high performance in the next generation of intelligent lighting systems with its portfolio of lighting IC products which include wireless solutions, LED drivers, intelligent occupancy sensors/DSPs, and energy measurement. More...

  • Heating, Ventilation & Air Conditioning
  • The comfort of a building's occupants is a top priority of any property manager. However, in today's environmentally conscious world it is a delicate balance between keeping people comfortable and conserving energy and operations costs. The best way to increase HVAC efficiency is to employ an accurate control and monitoring system. ADI offers complete signal chains to implement a variety of integrated, high quality HVAC control systems. More...

  • White Goods & Vending
  • Today's White Goods include more advanced elecronic user interfaces and displays, while at the same time becoming more energy efficient. Major Home Appliances of the future will also increasingly include wireless or wired connectivity options to allow seamless integration into Home Energy Management Systems. Through increased efficiency, connectivity, and control, household and building energy costs will thus be reduced without sacrificing performance. More...

RS-485 EMC

Featured Products

  • ADF7242

    The ADF7242 is a highly integrated, low power, and high performance transceiver for operation in the global 2.4 GHz ISM band. It is designed with emphasis on flexibility, robustness, ease of use, and low current consumption. The IC supports the IEEE 802.15.4-2006 2.4 GHz PHY requirements as well as proprietary GFSK/ FSK/GMSK/MSK modulation schemes in both packet and data streaming modes. With a MoreRead more

    ADF7242 Diagram

    - Low Power IEEE 802.15.4/Proprietary GFSK/FSK Zero-IF 2.4 GHz Transceiver IC

  • AD8495

    The AD8494/AD8495/AD8496/AD8497 are precision instrumentation amplifiers with thermocouple cold junction compensators on an integrated circuit. They produce a high level (5 mV/°C) output directly from a thermocouple signal by combining an ice point reference with a precalibrated amplifier. They can be used as standalone thermometers MoreRead more

    Functional Block Diagram

    - Full K-Type Range 0° to 50° Thermocouple Amplifier w/Cold Junction Compensation

  • AD7171

    The AD7171 is a very low power 16-bit analog-to-digital converter (ADC). It contains a precision 16-bit Σ-Δ ADC and an on-chip oscillator. Consuming only 110 μA, the AD7171 is particularly suitable for portable or battery operated products where very low power is a requirement. The AD7171 also has a power down mode in which the device consumes 5 μA, thus increasing the battery life of the MoreRead more

    Functional Block Diagram for AD7171

    - 16-Bit Low Power Σ−Δ ADC

  • ADF7023

    The ADF7023 is a very low power, high performance, highly integrated 2FSK/GFSK/OOK/MSK/GMSK transceiver designed for operation in the 862 MHz to 928 MHz and 431 MHz to 464 MHz frequency bands, which cover the worldwide license-free ISM bands at 433 MHz, 868 MHz, and 915 MHz. It is suitable for circuit applications that operate under the European ETSI EN300-220, the North American FCC (Part 15), MoreRead more

    ADF7023 Diagram

    - High Performance, Low Power, ISM Band FSK/GFSK/OOK/MSK/GMSK Transceiver IC

Featured Video:

ADI Shows Modular Wireless Sensor Network (WSN)


ADI Shows Modular Wireless Sensor Network (WSN)

The WSN demo system from Analog Devices is used to demonstrate a complete ISM band network. This kit provides complete out-of-the-box functionality and includes a base station node along with sensor nodes that support several sensor types.

View Video >>

Send Feedback X

Send Feedback

Close